IMX8M Mini secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Mini secure boot

1,905件の閲覧回数
filipvuko
Contributor I

Hi everyone,


I'm trying to wrap my head around building yocto image with secure boot for IMX 8M mini. So far researching google has lead me to a lot of 404 links and other dead ends. Can you please provide me with some guidance? 

 

Thank you

0 件の賞賛
返信
3 返答(返信)

1,879件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

You can refer to <10.9 Automated image signing for secure boot in i.MX application processors> from the Linux User Guide: i.MX Linux User's Guide (nxp.com.cn)

 

Regards

Harvey

0 件の賞賛
返信

1,865件の閲覧回数
filipvuko
Contributor I

What kind of security features are there on imx 8m mini and plus? 

For example:
HABv4?
CAAM? 
etc...

0 件の賞賛
返信

1,844件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Yes, there are security features, HABV4, CAAM...etc. You can refer to the corresponding SRM for different chip for more details.

Download Security Reference Manual for i.MX 8M Mini Applications Processor (nxp.com)

 

Regards

Harvey

0 件の賞賛
返信