IMX8M MINI Power Consumption Calculations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M MINI Power Consumption Calculations

Jump to solution
4,031 Views
jming
Contributor II

Hi,

Could you please let me know, How to calculate the power consumption in IMX8M mini processor,  I have an IMX8M mini design. The peripherals only use a camera with a CSI interface and Micro SD card. The power consumption of this design is a bit large, reaching 3.2W.  So how to Reduce SoC Power when only Running A53 on i.MX8M mini. 

Thank & Regards,

0 Kudos
Reply
1 Solution
4,015 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3 Replies
4,016 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3,612 Views
Mihir2
Contributor II

Hi NXP team,

 

We are using 'MIMX8MM5CVTKZAA' part in our design, without VPU.

 

The attached Appnote AN12410 is a good reference point for our design.

Appnote provides all the relevant power consumption for 'VDD_GPU_VPU_DRAM' power supply rail. If VPU is not being used, how shall we treat power consumption on these rails.

 

For example, Table-3 'IDLE_DEFAULT' condition in the appnote has a total current on 'VDD_GPU_VPU_DRAM' as 402 mA. 

Mihir2_0-1677219244536.png

How shall we consider the current?

1. 402 mA current on each VDD_GPU and VDD_DRAM power supply rails. 0mA on VDD_VPU.

2. 201 mA current on each VDD_GPU and VDD_DRAM rails and 0mA on VDD_VPU.

 

Regards,

Mihir

Tags (1)
0 Kudos
Reply
3,998 Views
jming
Contributor II

@Rita_Wang 

Thank you,

This is a good reference, we are testing. 

Tags (1)
0 Kudos
Reply