IMX8M Android Yocto Project fails to compile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Android Yocto Project fails to compile

ソリューションへジャンプ
2,331件の閲覧回数
baijinlong
Contributor III
            IMX8M Android source code compilation error, found in the DOC file configuration environment variables can not find build /envsetup.sh script, download the Yocto Project is not (I suspect missing).
pastedImage_1.png
         so the following configuration to add build / blueprint, build / core, prebuilts /build-tools, prebuilts/go and other tools and files (all missing).
pastedImage_2.png
         It is normal to execute the build/envsetup.sh and lunch evk_8mq-userdebug commands after adding the corresponding tools and files.
pastedImage_3.png
         However, when using make to compile the Yocto Project, an error occurs. I don't know what the situation is. The compile-generated out/soong/make_vars-evk_8mq.mk file still cannot be generated. It is the same result through many download attempts, or the lack of files and tools. The above error still occurs after manual replenishment.
pastedImage_4.png
·            What is this problem? I hope I can get support. Thank you!
ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,969件の閲覧回数
coindu
Contributor IV

Hi Bai,

    The same error i also encountered.  Because of the android source_code download  incomplete

元の投稿で解決策を見る

2 返答(返信)
1,970件の閲覧回数
coindu
Contributor IV

Hi Bai,

    The same error i also encountered.  Because of the android source_code download  incomplete

1,969件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Bai,

You are trying to compile yocto in Android? thats not going to happend you need to download the proper yocto for it.

0 件の賞賛
返信