IMX8_NAND_64Page_Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8_NAND_64Page_Boot

2,790 次查看
karimbakir
Contributor II

I have custom board  using imx8qxp mek board and I have in my board external NAND chip with 64 page . Also no boot switches match booting from NAND with 64 page . 

I dumped all fuses values in my board using uboot command :

#fuse read 0 0 0x10C 

So I have to burn eFuses to boot from NAND with 64 page , I check in the data sheet and I found i have to write in word 2 block 0 ,so I want to know is the following values is the correct value to boot form NAND with 64 page so I just run the following command in uboot :


#fuse prog -y 0 2 0x3001000A

//bank=0 word=2 value=0x3001000A (override NAND pages in block && configure 64 page per block ) .

Also I need to know Do i need to configure BT_MODE_FUSES [5:0] ? 

标记 (1)
0 项奖励
回复
2 回复数

2,588 次查看
b36401
NXP Employee
NXP Employee

Actually i.MX8QXP processor is not officially launched and not officially supported.

Please create a technical case:
https://community.nxp.com/thread/381898

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,588 次查看
karimbakir
Contributor II

I tried to burn the fuses using uboot command and I got the following error :

pastedImage_1.png

So how to burn eFuses using mfg tool , i tried the following command in u-boot but it does not work 

<CMD state="Updater" type="push" body="$ ls -l /sys/fsl_otp/">List fuses</CMD>
0 项奖励
回复