IMX8 Mini Bluetooth A2DP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 Mini Bluetooth A2DP

5,491 Views
ebecam
Contributor II

Hello,

I am using IMX8 Mini EVK and I try to play music using Bluetooth AD2P.


So far, I am able to pair and connect to my Bluetooth speaker.

Output of bluetoothctl:
[BAM Headset 00013]# info 20:71:9B:10:00:13
Device 20:71:9B:10:00:13 (public)
    Name: BAM Headset 00013
    Alias: BAM Headset 00013
    Class: 0x00240418
    Icon: audio-card
    Paired: yes
    Trusted: yes
    Blocked: no
    Connected: yes
    LegacyPairing: no
    UUID: Serial Port               (00001101-0000-1000-8000-00805f9b34fb)
    UUID: Audio Sink                (0000110b-0000-1000-8000-00805f9b34fb)
    UUID: A/V Remote Control Target (0000110c-0000-1000-8000-00805f9b34fb)
    UUID: A/V Remote Control        (0000110e-0000-1000-8000-00805f9b34fb)
    UUID: Handsfree                 (0000111e-0000-1000-8000-00805f9b34fb)
    UUID: PnP Information           (00001200-0000-1000-8000-00805f9b34fb)
    Modalias: bluetooth:v000Fp0401d0001

I tested the speaker with my Ubuntu laptop and it is working well in AD2P mode.

I launched pulseaudio in system mode and I can see from the logs that bluetooth modules are loaded:
# pulseaudio -vvvv --system
...
I: [pulseaudio] module.c: Loaded "module-bluez5-discover" (index: #11; argument: "").
D: [pulseaudio] module.c: Checking for existence of '/usr/lib/pulse-11.1/modules/module-bluez4-discover.so': failure
I: [pulseaudio] module.c: Loaded "module-bluetooth-discover" (index: #10; argument: "").
I: [pulseaudio] module.c: Loaded "module-bluetooth-policy" (index: #12; argument: "").
I: [pulseaudio] module.c: Loaded "module-switch-on-connect" (index: #13; argument: "").
D: [pulseaudio] main.c: Got org.pulseaudio.Server!
I: [pulseaudio] main.c: Daemon startup complete.
....

The Bluetooth sound card is detected correctly under pulseaudio:
# pactl list cards
Card #1
    Name: bluez_card.20_71_9B_10_00_13
    Driver: module-bluez5-device.c
    Owner Module: 16
    Properties:
        device.description = "BAM Headset 00013"
        device.string = "20:71:9B:10:00:13"
        device.api = "bluez"
        device.class = "sound"
        device.bus = "bluetooth"
        device.form_factor = "headphone"
        bluez.path = "/org/bluez/hci0/dev_20_71_9B_10_00_13"
        bluez.class = "0x240418"
        bluez.alias = "BAM Headset 00013"
        device.icon_name = "audio-headphones-bluetooth"
    Profiles:
        a2dp_sink: High Fidelity Playback (A2DP Sink) (sinks: 1, sources: 0, priority: 10, available: yes)
        headset_head_unit: Headset Head Unit (HSP/HFP) (sinks: 1, sources: 1, priority: 20, available: no)
        off: Off (sinks: 0, sources: 0, priority: 0, available: yes)
    Active Profile: a2dp_sink
    Ports:
        headphone-output: Headphone (priority: 0, latency offset: 0 usec, available)
            Part of profile(s): a2dp_sink, headset_head_unit
        headphone-input: Bluetooth Input (priority: 0, latency offset: 0 usec, not available)
            Part of profile(s): headset_head_unit
            
            
# pactl list sinks
Sink #5
    State: IDLE
    Name: bluez_sink.20_71_9B_10_00_13.a2dp_sink
    Description: BAM Headset 00013
    Driver: module-bluez5-device.c
    Sample Specification: s16le 2ch 48000Hz
    Channel Map: front-left,front-right
    Owner Module: 18
    Mute: no
    Volume: front-left: 65536 / 100% / 0.00 dB,   front-right: 65536 / 100% / 0.00 dB
            balance 0.00
    Base Volume: 65536 / 100% / 0.00 dB
    Monitor Source: bluez_sink.20_71_9B_10_00_13.a2dp_sink.monitor
    Latency: 43009 usec, configured 38333 usec
    Flags: HARDWARE DECIBEL_VOLUME LATENCY
    Properties:
        bluetooth.protocol = "a2dp_sink"
        device.description = "BAM Headset 00013"
        device.string = "20:71:9B:10:00:13"
        device.api = "bluez"
        device.class = "sound"
        device.bus = "bluetooth"
        device.form_factor = "headphone"
        bluez.path = "/org/bluez/hci0/dev_20_71_9B_10_00_13"
        bluez.class = "0x240418"
        bluez.alias = "BAM Headset 00013"
        device.icon_name = "audio-headphones-bluetooth"
    Ports:
        headphone-output: Headphone (priority: 0, available)
    Active Port: headphone-output
    Formats:
        pcm


Trouble appear when I try to play a file.
Here is the command launched to play a 1kHz tone:
# paplay -v /usr/share/soundcard-test-config/tone_1000.wav
Opening a playback stream with sample specification 's16le 2ch 48000Hz' and channel map 'front-left,front-right'.
Connection established.
Stream successfully created.
Buffer metrics: maxlength=4194304, tlength=384000, prebuf=380164, minreq=3840
Using sample spec 's16le 2ch 48000Hz', channel map 'front-left,front-right'.
Connected to device bluez_sink.20_71_9B_10_00_13.a2dp_sink (index: 1, suspended: no).
Stream started.
Playback stream drained.y: 5517 usec.           
Draining connection to server.


Below are the logs of pulseaudio -vvvv --system:
D: [pulseaudio] sink-input.c: Negotiated format: pcm, format.sample_format = "\"s16le\""  format.rate = "48000"  format.channels = "2"  format.channel_map = "\"front-left,front-right\""
I: [pulseaudio] sink-input.c: Trying to change sample rate
D: [pulseaudio] module-suspend-on-idle.c: Sink bluez_sink.20_71_9B_10_00_13.a2dp_sink becomes busy, resuming.
D: [pulseaudio] resampler.c: Resampler:
D: [pulseaudio] resampler.c:   rate 48000 -> 44100 (method ffmpeg)
D: [pulseaudio] resampler.c:   format s16le -> s16le (intermediate s16le)
D: [pulseaudio] resampler.c:   channels 2 -> 2 (resampling 2)
D: [pulseaudio] memblockq.c: memblockq requested: maxlength=33554432, tlength=0, base=4, prebuf=0, minreq=1 maxrewind=0
D: [pulseaudio] memblockq.c: memblockq sanitized: maxlength=33554432, tlength=33554432, base=4, prebuf=0, minreq=4 maxrewind=0
I: [pulseaudio] sink-input.c: Created input 0 "/usr/share/soundcard-test-config/tone_1000.wav" on bluez_sink.20_71_9B_10_00_13.a2dp_sink with sample spec s16le 2ch 48000Hz and channel map front-left,front-right
I: [pulseaudio] sink-input.c:     media.format = "WAV (Microsoft)"
I: [pulseaudio] sink-input.c:     application.name = "paplay"
I: [pulseaudio] sink-input.c:     media.name = "/usr/share/soundcard-test-config/tone_1000.wav"
I: [pulseaudio] sink-input.c:     native-protocol.peer = "UNIX socket client"
I: [pulseaudio] sink-input.c:     native-protocol.version = "32"
I: [pulseaudio] sink-input.c:     application.process.id = "3791"
I: [pulseaudio] sink-input.c:     application.process.user = "root"
I: [pulseaudio] sink-input.c:     application.process.host = "imx8mmevk"
I: [pulseaudio] sink-input.c:     application.process.binary = "pacat"
I: [pulseaudio] sink-input.c:     application.language = "C"
I: [pulseaudio] sink-input.c:     application.process.machine_id = "95dd73e1a8bd4e43ad491e0a02f38899"
I: [pulseaudio] sink-input.c:     module-stream-restore.id = "sink-input-by-application-name:paplay"
I: [pulseaudio] protocol-native.c: Requested tlength=2000.00 ms, minreq=20.00 ms
D: [pulseaudio] protocol-native.c: Traditional mode enabled, modifying sink usec only for compat with minreq.
D: [pulseaudio] protocol-native.c: Requested latency=1960.00 ms, Received latency=39.51 ms
D: [pulseaudio] memblockq.c: memblockq requested: maxlength=4194304, tlength=384000, base=4, prebuf=380164, minreq=3840 maxrewind=0
D: [pulseaudio] memblockq.c: memblockq sanitized: maxlength=4194304, tlength=384000, base=4, prebuf=380164, minreq=3840 maxrewind=0
I: [pulseaudio] protocol-native.c: Final latency 2039.51 ms = 1960.00 ms + 2*20.00 ms + 39.51 ms
I: [pulseaudio] module-stream-restore.c: Storing volume/mute/device for stream sink-input-by-application-name:paplay.
D: [pulseaudio] protocol-dbus.c: Interface org.PulseAudio.Ext.StreamRestore1.RestoreEntry added for object /org/pulseaudio/stream_restore1/entry1
D: [bluetooth] protocol-native.c: Requesting rewind due to end of underrun.
W: [bluetooth] module-bluez5-device.c: Skipping 28873 us (= 5092 bytes) in audio stream
D: [bluetooth] module-bluez5-device.c: Bitpool has changed to 48
W: [bluetooth] module-bluez5-device.c: Skipping 273889 us (= 48312 bytes) in audio stream
D: [bluetooth] module-bluez5-device.c: Bitpool has changed to 43
W: [bluetooth] module-bluez5-device.c: Skipping 100358 us (= 17700 bytes) in audio stream
D: [bluetooth] module-bluez5-device.c: Bitpool has changed to 38
W: [bluetooth] module-bluez5-device.c: Skipping 506565 us (= 89356 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 89356 > 65536
D: [bluetooth] module-bluez5-device.c: Bitpool has changed to 33
W: [bluetooth] module-bluez5-device.c: Skipping 450721 us (= 79504 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79504 > 65536
D: [bluetooth] module-bluez5-device.c: Bitpool has changed to 32
W: [bluetooth] module-bluez5-device.c: Skipping 448194 us (= 79060 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79060 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 450855 us (= 79528 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79528 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 452899 us (= 79888 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79888 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 397041 us (= 70036 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 70036 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 429440 us (= 75752 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 75752 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 462023 us (= 81500 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 81500 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453250 us (= 79952 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79952 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 370121 us (= 65288 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 435722 us (= 76860 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 76860 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 410607 us (= 72428 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 72428 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 440766 us (= 77748 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 77748 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 458204 us (= 80824 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 80824 > 65536
I: [pulseaudio] module-stream-restore.c: Synced.
W: [bluetooth] module-bluez5-device.c: Skipping 450733 us (= 79508 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79508 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 441875 us (= 77944 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 77944 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 382041 us (= 67392 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 67392 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453100 us (= 79924 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79924 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 467110 us (= 82396 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 82396 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 429388 us (= 75744 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 75744 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453252 us (= 79952 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79952 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 415780 us (= 73340 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 73340 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 428072 us (= 75508 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 75508 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 450703 us (= 79504 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79504 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 466999 us (= 82376 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 82376 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 450588 us (= 79480 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79480 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 385765 us (= 68048 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 68048 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 443201 us (= 78180 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 78180 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 450698 us (= 79500 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79500 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453122 us (= 79928 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79928 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 452083 us (= 79744 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79744 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 410774 us (= 72460 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 72460 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 428039 us (= 75504 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 75504 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 454423 us (= 80160 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 80160 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 373923 us (= 65960 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 65960 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453201 us (= 79944 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79944 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453272 us (= 79956 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79956 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 389529 us (= 68712 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 68712 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453024 us (= 79912 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79912 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 448205 us (= 79060 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79060 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 455692 us (= 80384 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 80384 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 428277 us (= 75548 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 75548 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 410727 us (= 72452 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 72452 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 450585 us (= 79480 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79480 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453285 us (= 79956 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79956 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 445720 us (= 78624 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 78624 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 453124 us (= 79928 bytes) in audio stream
D: [bluetooth] memblock.c: Memory block too large for pool: 79928 > 65536
W: [bluetooth] module-bluez5-device.c: Skipping 19310 us (= 3404 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86867 us (= 15320 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86820 us (= 15312 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86770 us (= 15304 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86776 us (= 15304 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 19261 us (= 3396 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 98109 us (= 17304 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 90700 us (= 15996 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 61578 us (= 10860 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86757 us (= 15300 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 44234 us (= 7800 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 61976 us (= 10932 bytes) in audio stream
D: [bluetooth] protocol-native.c: Implicit drain of '/usr/share/soundcard-test-config/tone_1000.wav'
D: [bluetooth] protocol-native.c: Drain acknowledged of '/usr/share/soundcard-test-config/tone_1000.wav'
I: [pulseaudio] sink-input.c: Freeing input 0 "/usr/share/soundcard-test-config/tone_1000.wav"
I: [pulseaudio] client.c: Freed 2 "paplay"
I: [pulseaudio] protocol-native.c: Connection died.
W: [bluetooth] module-bluez5-device.c: Skipping 86604 us (= 15276 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86885 us (= 15324 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86767 us (= 15304 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 44380 us (= 7828 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 63056 us (= 11120 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86867 us (= 15320 bytes) in audio stream
W: [bluetooth] module-bluez5-device.c: Skipping 86612 us (= 15276 bytes) in audio stream

There is no audio coming out the Bluetooth speaker and after a few minutes I hear crackling audio coming from my Bluetooth speaker.

I turn on logs for the bluetoothd service by passing the -d option to the command line but I don't see logs that can help me.


Do you have any idea what could cause those issue ? Is there some pulseaudio configurations that could fix it ?

Thanks for your help !

Labels (1)
0 Kudos
Reply
2 Replies

4,842 Views
ebecam
Contributor II

I finally got the A2DP Bluetooth working.

The UART speed used for Bluetooth was 115200.

When using the command hciattach /dev/ttymxc0 qca 3000000 flow -b -t 120 documented in the i.MX Linux User's Guide, I have no more audio issue when playing music from the IMX Evaluation Board to my Bluetooth speaker.

The UART for the Bluetooth has now the following configuration:

# stty -F /dev/ttymxc0                                                                                                        
speed 3000000 baud; line = 15;
min = 1; time = 0;
-brkint -icrnl -imaxbel
-opost
-isig -icanon -iexten -echo

I now try to to sent AVRCP commands for volume down/up. Do you have any tips or guidelines for this ?

For now, I check the volume with the command "pactl list sinks" and I looked at the "Volume" line.

However, when pressing the Volume + and Volume - button of my Bluetooth speaker, the volume given by pactl does not change.

For information, I build using the core-image-base.

Thanks

0 Kudos
Reply

4,842 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

You can do it with amixer.

First, reproduce the track in background process.

Then, configure amixer as below to increase the volume:

amixer -D pulse sset Master <your desired percentage of volume to increase>% + #note that default volume is at 100% percent‍

To lower the volume configure amixer as below:

amixer -D pulse sset Master <your desired percentage of volume to decrease>% -‍

And to set a default volume configure amixer as below:

amixer -D pulse sset Master <your desired percentage of volume to increase>% ‍

Hope this information could help you.

Best regards,

Diego.

0 Kudos
Reply