IMX8 MIPI CSI RAW14 mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 MIPI CSI RAW14 mode

4,025 Views
james_kim
Contributor II

Hi,

Does anyone  get it working at CSI RAW14 mode? I have been working successfully RAW 8/10/12 mode.

I'm getting in data but it was corrupted. 

James

0 Kudos
Reply
3 Replies

3,848 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the Reference Manual:

Image Sensing Interface (ISI):

• Stream Manipulation Features
• Supported Pixel Formats when storing image into memory
• RAW8, RAW10, RAW12, RAW16
• RGB888, BGR888, RGB565, RGB 10-bit, BGR 10-bit
• YUV444, YUV422, YUV420 (8-bit, 10-bit, 12-bit)
• Plus more formats listed in the description of FORMAT field in the
channel's IMG_CTRL register

0 Kudos
Reply

3,849 Views
james_kim
Contributor II

It is working now.

James

0 Kudos
Reply

1,822 Views
mjp111
Contributor I

Could you elaborate, got RAW14 working in ISI path? What was the key?

0 Kudos
Reply