Hello,
According to app note "i.MX 7DS Power Consumption Measurement" in system idle mode consumption
is ~52 mW. Using Thermal Resistance Data in the i.MX7D Datasheet for four-layer board; natural convection
(as 30.2 C / W) rough estimation of temperature is T ambient + 1.5 C
Note, to enter idle mode, as stated in section 6.2.3 (System Idle mode: system setup) of the app note:
Disconnect everything except for the SD.
1. Boot up the Linux image by entering “x11=false uart_from_osc” into the command line.
2. Run the following script to put the system into the “powersave” governor:
#!/bin/bash
echo 8 > /proc/sys/kernel/printk
ifconfig eth0 down ifconfig eth1 down
echo powersave > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor echo 1 > /sys/class/graphics/fb0/blank
3. Measure the power and record the result.
https://www.nxp.com/docs/en/application-note/AN5383.pdf
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.