IMX7D, LPDDR3 register setting Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D, LPDDR3 register setting Query

880 Views
logeshs
Contributor II

Hi,

We are using IMX7D (MCIMX7D3EVK10SD) in our board along with Kingston LPDDR3 (08EMCP08-EL3DT227-A01U). I'm filling out the (MX7D_LPDDR3_register_programming_aid_v1_4) Register Programming sheet. I have below query in DDRC_DRAMTMG4 register,

1. What should I want to fill under T_RP? It is mentioned as Same Bank in below description, Please confirm should i want to use Precharge time for One Bank or All banks (Please find the attachment for Datasheet snip)

1. 

T_RP21/18700000007Note, the user must supply the tRP (in ns) value from the DRAM data sheet.
Description: tRP: Minimum time from precharge to activate of same bank.
Since this design is configured with MEMC_FREQ_RATIO=2, t_rp should be set to RoundDown(RoundUp(tRP/tCK)/2) + 1. (this is performed automatically)
Unit: Clocks.
Value After Reset: 0x5

Please confirm as soon as possible. Thanks

Labels (1)
0 Kudos
Reply
2 Replies

757 Views
igorpadykov
NXP Employee
NXP Employee

Hi Logesh

please use Precharge time for One Bank parameter.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

757 Views
logeshs
Contributor II

Igor,

Thank you so much.

Regards,

Logesh

0 Kudos
Reply