IMX7- MCIMX7 SABRE Cellular modem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX7- MCIMX7 SABRE Cellular modem

1,677 次查看
syamkrishnan_m
Contributor II


Hi,

I'm looking for any software support for a Cellular modem connected to IMX7- MCIMX7 SABRE platform using a Linux distribution. Anyone having any knowledge about what is already supported regarding API's and interfaces such as USB, PCIe to connect an external modem that could be accesses via an application or command line. Request for some suggestions for using GSM with my MY SABRE BOARD FOR a POC.
Thanks,
Sam

标签 (1)
0 项奖励
回复
2 回复数

1,576 次查看
syamkrishnan_m
Contributor II

Thanks Igor..Ihave connected SIM800 GSM module and got the messaging working using AT Commands.

Thanks,

Syam

0 项奖励
回复

1,576 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sam

one can look at boundary devices modem resources and try to use it for i.MX7

Cellular modems on i.MX6 boards under Ubuntu - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复