IMX7- MCIMX7 SABRE Cellular modem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7- MCIMX7 SABRE Cellular modem

1,645 Views
syamkrishnan_m
Contributor II


Hi,

I'm looking for any software support for a Cellular modem connected to IMX7- MCIMX7 SABRE platform using a Linux distribution. Anyone having any knowledge about what is already supported regarding API's and interfaces such as USB, PCIe to connect an external modem that could be accesses via an application or command line. Request for some suggestions for using GSM with my MY SABRE BOARD FOR a POC.
Thanks,
Sam

Labels (1)
0 Kudos
Reply
2 Replies

1,544 Views
syamkrishnan_m
Contributor II

Thanks Igor..Ihave connected SIM800 GSM module and got the messaging working using AT Commands.

Thanks,

Syam

0 Kudos
Reply

1,544 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sam

one can look at boundary devices modem resources and try to use it for i.MX7

Cellular modems on i.MX6 boards under Ubuntu - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply