IMX6ul elcdif/lcdif linux source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ul elcdif/lcdif linux source

2,471件の閲覧回数
ameerhamza
Contributor III

Hi all,

I want to ask if the source code is freely available for imx6ul elcdif linux driver. If yes where can i get the source from. Any help would be appreciated.

Thanks,

Am Hamza.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,925件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Am

please refer to Chapter 12 ELCDIF Frame Buffer Driver

attached Linux Manual, sources link

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/?h=imx_4.1.15_1.0.0_ga

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信