sorry, I don't understand. which logo you want to change?
i have changed the logo,and follow freescale's patch keep uboot logo to kernel.however, when show to the android logo(which we called third logo),the screen has a splash.
now,do understand?
which bsp are you using?
JB4.2.2_1.1.0,this is my kernel log.
W/imx6.gralloc( 2427): id = DISP3 BG
W/imx6.gralloc( 2427): xres = 1024 px
W/imx6.gralloc( 2427): yres = 768 px
W/imx6.gralloc( 2427): xres_virtual = 1024 px
W/imx6.gralloc( 2427): yres_virtual = 2304 px
W/imx6.gralloc( 2427): bpp = 32
W/imx6.gralloc( 2427): r = 0:8
W/imx6.gralloc( 2427): g = 8:8
W/imx6.gralloc( 2427): b = 16:8
W/imx6.gralloc( 2427): width = 163 mm (159.568100 dpi)
W/imx6.gralloc( 2427): height = 122 mm (159.895081 dpi)
W/imx6.gralloc( 2427): refresh rate = 60.00 Hz
I/FslHwcomposer( 2427): fb0 is ldb
I/FslHwcomposer( 2427): device
I/FslHwcomposer( 2427): fb1 is overlay device
W/FslHwcomposer( 2427): open /sys/class/graphics/fb2 failed
W/FslHwcomposer( 2427): open /sys/class/graphics/fb3 failed
W/FslHwcomposer( 2427): open /sys/class/graphics/fb4 failed
W/FslHwcomposer( 2427): open /sys/class/graphics/fb5 failed
I/FslHwcomposer( 2427): hwcomposer: open framebuffer fb0
I/mediaserver( 2430): ServiceManager: 0x418d7000
I/AudioFlinger( 2430): Using default 3000 mSec as standby time.
I/CameraService( 2430): CameraService started (pid=2430)
W/v_hwc ( 2427): TODO: HWC integration: display!
I/v_hwc ( 2427): Default primary display
I/v_hwc ( 2427): xres = 1024 px
I/v_hwc ( 2427): yres = 768 px
I/v_hwc ( 2427): xdpi = 159.6 dpi
I/v_hwc ( 2427): ydpi = 159.9 dpi
I/v_hwc ( 2427): refresh rate = 60.0 Hz
E/v_hwc ( 2427): open /dev/graphics/fb2 failed
I/v_hwc ( 2427): Virtual display 0 initialized.
I/v_hwc ( 2427): Vivante HWComposer v2.4
I/v_hwc ( 2427): Device: 0x41c0f2a0
I/v_hwc ( 2427): Separated 2D: YES
I/v_hwc ( 2427): 2D PE20: YES
I/v_hwc ( 2427): Multi-source blit: NO
I/v_hwc ( 2427): Multi-source blit Ex: NO
I/v_hwc ( 2427): OPF/YUV blit/Tiling : NO
I/v_hwc ( 2427): Filter stretch : YES
I/FslHwcomposer( 2427): hwc_device_open,367
I/SurfaceFlinger( 2427): Using composer version 1.1
W/SurfaceFlinger( 2427): no suitable EGLConfig found, trying without EGL_FRAMEBUFFER_TARGET_ANDROID
I/FslCameraHAL( 2430): Face Back Camera is ov5640_mipi, orient is 0
I/FslCameraHAL( 2430): Face Front Camera is mt9d115_csi_camera, orient is 0
I/FslCameraHAL( 2430): Checking the camera ov5640_mipi
I/FslCameraHAL( 2430): Checking the camera mt9d115_csi_camera
E/SurfaceFlinger( 2427): HWComposer: framebufferTarget is null
E/SurfaceFlinger( 2427): HWComposer: framebufferTarget is null
W/GraphicBufferAllocator( 2427): WOW! gralloc alloc failed, waiting for pending frees!
E/SurfaceFlinger( 2427): HWComposer: framebufferTarget is null
E/SurfaceFlinger( 2427): HWComposer: framebufferTarget is null
E/libEGL ( 2427): eglSetSwapRectangleANDROID:1318 error 3008 (EGL_BAD_DISPLAY)
I/SurfaceFlinger( 2427): EGL informations:
I/SurfaceFlinger( 2427): vendor : Android
I/SurfaceFlinger( 2427): version : 1.4 Android META-EGL
I/SurfaceFlinger( 2427): extensions: EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_renderbuffer_image EGL_KHR_fence_sync EGL_ANDROID_image_native_buffer
I/SurfaceFlinger( 2427): Client API: OpenGL_ES
I/SurfaceFlinger( 2427): EGLSurface: 8-8-8-8, config=0x408d1d38
I/SurfaceFlinger( 2427): OpenGL ES informations:
I/SurfaceFlinger( 2427): vendor : Vivante Corporation
I/SurfaceFlinger( 2427): renderer : GC880 Graphics Engine
I/SurfaceFlinger( 2427): version : OpenGL ES-CM 1.1
I/SurfaceFlinger( 2427): extensions: GL_EXT_debug_marker GL_OES_blend_equation_separate GL_OES_blend_func_separate GL_OES_blend_subtract GL_OES_byte_coordinates GL_OES_compressed_ETC1_RGB8_texture GL_OES_compressed_paletted_texture GL_OES_draw_texture GL_OES_extended_matrix_palette GL_OES_fixed_point GL_OES_framebuffer_object GL_OES_matrix_get GL_OES_matrix_palette GL_OES_point_size_array GL_OES_point_sprite GL_OES_query_matrix GL_OES_read_format GL_OES_single_precision GL_OES_stencil_wrap GL_OES_texture_cube_map GL_OES_texture_mirrored_repeat GL_OES_EGL_image GL_OES_depth24 GL_OES_element_index_uint GL_OES_fbo_render_mipmap GL_OES_mapbuffer GL_OES_rgb8_rgba8 GL_OES_stencil1 GL_OES_stencil4 GL_OES_stencil8 GL_OES_texture_npot GL_OES_vertex_half_float GL_OES_packed_depth_stencil GL_EXT_texture_format_BGRA8888 GL_IMG_read_format GL_IMG_user_clip_plane GL_APPLE_texture_2D_limited_npot GL_EXT_texture_lod_bias GL_EXT_blend_minmax GL_EXT_read_format_bgra GL_EXT_multi_draw_arrays GL_OES_EGL_sync GL_APPLE_texture_format_BGRA8888 GL_APPLE_te
I/SurfaceFlinger( 2427): GL_MAX_TEXTURE_SIZE = 8192
I/SurfaceFlinger( 2427): GL_MAX_VIEWPORT_DIMS = 8192 x 8192
I/AudioPolicyManagerBase( 2430): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2430): card 0, id wm8962audio ,driver wm8962-audio, name wm8962-audio
W/audio_hw_primary( 2430): out rate 44100
W/audio_hw_primary( 2430): in rate 44100, channels 1 format 0
D/SurfaceFlinger( 2427): Screen acquired, type=0 flinger=0x41c0e318
I/AudioFlinger( 2430): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2430): open output stream devices 2, format 1, channels 3, sample_rate 44100, flag 2
W/audio_hw_primary( 2430): opened out stream...1075390832
I/AudioFlinger( 2430): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2430): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2430): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
D/libEGL ( 2653): loaded /system/lib/egl/libEGL_VIVANTE.so
D/libEGL ( 2653): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so
D/libEGL ( 2653): loaded /system/lib/egl/libGLESv2_VIVANTE.so
E/BufferQueue( 2427): [BootAnimation] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count
E/BootAnimation( 2653): [aaron]:**********add for test
So, you want to keep the 'Android' logo? or not?
if not, please try to remove the bootanimation in the init.rc.
no,
we have two logo,one is uboot logo,the other is the android logo,however when the uboot logo turn to be android logo,the screen has a flash which is so ungainly,can you tell me how to deal with it????
The issue should be caused by your modification on the patch, please list your modifications.
Dear li:
i attempt to change the patch to yours,but i find it is hold on the kernel start........,can you give some tips?
they say that you are the master of this part .
What's your display config? LVDS panel on LVDS port 0? Are you use JB4.2.2 BSP?
yes,lvds_num=0,but did that relation to the ipu di? I think the ipu dix can transform for lvds0 and lvds1. did this right?
i was use JB4.2.2 .and what's the meaning of display config?
static struct fb_videomode ldb_modedb[] = {
{
"LDB-PAT215", 60, 1024, 768,15385,
240, 48,
23, 3,
32, 12,
0 ,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
};
is this?
The LVDS0 example had been given in Patch to support uboot logo keep from uboot to kernel to Android for JB4.2.2_1.1.0-GA and L3.0.35_4....
Verified on both iMX6DQ and iMX6DL boards.
Dear li:
I find when i ptach your patch,it will stop at do_register_framebuffer
fb_notifier_call_chain(FB_EVENT_FB_REGISTERED, &event);
and previous my colleague delete this code. she has resigned. i don't know how she did that,
so i porting her code to my project. but my has ipu warning.
You should not change that code.
嗨,Dear Li,porting了你给的uboot里面的代码,修改了LVDS_NUM=0;DISP_NUM=0;但是屏幕一直黑屏,量取了信号,发现信号线没有信号出来,其他时钟电压都是ok的,请问是否是因为该patch不支持LVDS0的配置?
LVDS0的例子也已经给了,porting的工作都不需要了,你只要直接打patch,然后修改你们的LVDS屏用的timing参数就可以了。
嗨 li,我研究了你的patch,看你的patch在uboot里面应该默认就是支持LVDS1的吧,但是我这边是需要支持LVDS0,所以我顺便改了相应LVDS_NUM=0;DISP_NUM=0,应该是ok的吧,但是开启之后一直黑屏,所以想讨教下是否还需要改什么别的参数。
只要uboot头文件改LVDS_NUM=0;DISP_NUM=0,然后kernel编译时,也选成CONFIG_MX6_CLK_FOR_BOOTUI_TRANS_LVDS_IPU1_DI0,就好了。
Dear li:
打了你的patch无法显示,我这边把所有之前和现在的patch全部拿掉,结果发现还是会出现ipu_warning.但是概率有所下降。
具体发现ipu_warning发生的地方是在:
mxcfb_set_par中的4.4——4.5之间
printk("[4]\n");
ipu_clear_irq(mxc_fbi->ipu, mxc_fbi->ipu_ch_irq);
printk("[4.1]\n");
ipu_disable_irq(mxc_fbi->ipu, mxc_fbi->ipu_ch_irq);
printk("[4.2]\n");
ipu_clear_irq(mxc_fbi->ipu, mxc_fbi->ipu_ch_nf_irq);
printk("[4.3]\n");
ipu_disable_irq(mxc_fbi->ipu, mxc_fbi->ipu_ch_nf_irq);
printk("[4.4]\n");
ipu_disable_channel(mxc_fbi->ipu, mxc_fbi->ipu_ch, true);
printk("[4.5]\n");
ipu_uninit_channel(mxc_fbi->ipu, mxc_fbi->ipu_ch);
printk("[5.]\n");
所以我觉得和我打得patch应该是没什么关系吧?不知道您之前是否遇到过类似的问题?
请确保display和IPU相关的代码恢复到原始的BSP,再来测试。
或者你有Freescale开发板的话,最好现在开发板上试试在,针对你这个LVDS0的用法,我特地做了一个CONFIG_MX6_CLK_FOR_BOOTUI_TRANS_LVDS_IPU1_DI0的例子,都测试过没问题了。
嗨,li,现在的现象看来应该不是我打得patch问题,是否有其他模块干扰到display部分的可能呢?