IMX6ULL uboot failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL uboot failed

1,404件の閲覧回数
jax_wang
Contributor II

Hi everyone:

I  compiled uboot-2018 and used command `dd` to flash u-boot image, it outputs following

U-Boot 2018.03 (Dec 12 2022 - 15:46:27 +0800)

CPU:   Freescale i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 32C
Reset cause: POR
Model: Freescale i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM:  512 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
switch to partitions #0, OK
mmc0 is current device
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
Display: TFT7016 (1024x600)
Video: 1024x600x24
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc0 is current device
flash target is MMC:0
Net:   No ethernet found.
fastboot  key pressed
Fastboot: Got bootloader commands!

The SD card's partition is following guide

p [lists the current partitions]
d [to delete existing partitions. Repeat this until no
unnecessary partitions
are reported by the 'p' command to start fresh.]
n [create a new partition]
p [create a primary partition - use for both
partitions]
1 [the first partition]
20480 [starting at offset sector]
1024000 [ending position of the first partition to be used
for the boot images]
p [to check the partitions]
n
p
2
1228800 [starting at offset sector, which leaves enough space
for the kernel,
the bootloader and its configuration data]
<enter> [using the default value will create a partition that
extends to
the last sector of the media]
p [to check the partitions]
w [this writes the partition table to the media and
fdisk exits]

 What should i do next?

ラベル(1)
0 件の賞賛
返信
1 返信

1,368件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @jax_wang,

 

Please provide me with the following details,

  • The command that you are using to flash the u-boot image to the SD Card and the u-boot image name.
  • Please try rebuilding the u-boot image.

 

Thanks & Regards,
Dhruvit.

0 件の賞賛
返信