IMX6ULL supports systemd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL supports systemd

1,947件の閲覧回数
vasudhevan
Contributor V

Hi Team,

Processor = IMX6ULL

Currently we using sysvint.

can we use systemd, if we use systemd what are the disadvantages is there.

what is the major difference between systemd and sysvint  ?

Regards,

  Vasu

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,855件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

In the following web page you can find a very good comparison between both Init options:

https://linoxide.com/linux-command/systemd-vs-sysvinit-cheatsheet/ 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,855件の閲覧回数
vasudhevan
Contributor V

Hi Jamesbone,

Thank You for your response.

I having one more doubt if we use systemd rootfs size increase except that performance wise any issue is there because of IMX6ULL is single core processor.

What is the status of CPU and RAM usage compared to sysvinit ?

Regards,

  Vasu

0 件の賞賛
返信