IMX6ULL Wakeup Source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL Wakeup Source

1,763件の閲覧回数
shammi112
Contributor I

Hello,

Can i use Any UART( out of 8) and GPIO  for wake-up from standby mode ?

Regards,

SHAMMI

0 件の賞賛
返信
1 返信

1,577件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, basically any UART supports wake up feature.

Look at section 55.4.2.3 (Clocking in Low-Power Modes) of i.MX 6ULL

Applications Processor Reference Manual, Rev. 1, 11/2017


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信