IMX6ULL-MCIMX6Y2CVM08AA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6ULL-MCIMX6Y2CVM08AA

2,000 次查看
baijinlong
Contributor III

               The EMMC clock CLK level is abnormal. Under normal conditions, it is 3.3v level. However, after measurement, it is found that the EMMC clock CLK voltage is always 1.8v. What is the situation? Hope to get your help, thank you!

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,379 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jinlong

one can check power supplies of eMMC signals with oscilloscope, if they are changing in

application, please look at Table 91. 14 x 14 mm Functional Contact Assignments for "Power Group"

i.MX6ULL Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf 

and check power supplies using Design Checklist

https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复