Hi,
We designed a monitoring system using IMX6ULL processor and 1GB DDR3 RAM. There is two DDR3 chips with 512MB.
But, the first DDR chip with chip select 0 (CS0) is neither good nor working properly.
If we are removing the Bad DDR chip1, then can we use the second DDR chip with CS0 by shorting DRAM_CS0 and DRAM_CS1 ?
Hi Dibin
shorting DRAM_CS0 and DRAM_CS1 is not allowed, in general one can try to debug
it with jtag (write/read to ddr memory locations and checking waveforms with oscilloscope)
using scripts from ddr test package
i.MX6/7 DDR Stress Test Tool V3.00
Other options may be running ddr test in lower frequencies and checking power supplies
ripples, should be < 5% as described in Hardware Development Guide for the i.MX6ULL
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------