IMX6ULL 5.0EMMC boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL 5.0EMMC boot?

1,780 Views
小辉哥
Contributor III

你好 请问IMX6ULL 支持5.0的emmc启动吗?我之前用的4.51的emmc可以启动 现在换了5.0的 可以用mfgtool烧写进去 但是不启动 支持进入烧写模式了,请问是需要别的设置吗?

Labels (3)
0 Kudos
Reply
2 Replies

1,633 Views
joanxie
NXP TechSupport
NXP TechSupport

try to change the source code in the drivers/mmc/core/mmc.c , change 6 to 7 in the "if (card->ext_csd.rev > 6)", then can support emmc 5.0

0 Kudos
Reply

1,633 Views
小辉哥
Contributor III

请问是在uboot下面change 还是linux下面,我使用的linux4.1.15 里面都已经改过来了。

0 Kudos
Reply