IMX6Sololite PCLK High Level DC input Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Sololite PCLK High Level DC input Voltage

1,987 Views
fisherhe
Contributor II

Hi,

    Customer now is using IMX6SOLOLITE, and they has a camera connect to imx6sl by CSI  module, and PCLK comes from camera to imx6. Now they want to know whether the High level DC input voltage(Vih) for PCLK is 0.7 x OVDD or 0.5 x OVDD? 

     In datasheet, there is a table as below:

1.png

  From this table, we can see is 0.7 x OVDD.

 But, in the chapter of CSI ,there are figures as below:

2.png

3.png

From Figure 23 and Table 37, It seems that the high time(P5) and low time (P6) of PCLK is calculateed from the middle of the wave, that is the point of 0.5 x VDD.

      So, now is the question, the Vih of PCLK is 0.7 x OVDD(OVDD is 3.3v now, that is 2.31v), or 0.5 x OVDD? Cutstomer want to know the lowest value of the PCLK high levle. Now they find that the peak of PCLK on their board is 2.2v and still work OK.

      Thank you!

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,931 Views
fisherhe
Contributor II

Thank you!

0 Kudos
Reply

1,931 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fisher

correct is Table 21 Datasheet.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply