IMX6Solo Deep sleep issue?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Solo Deep sleep issue?

3,335 Views
ramesh6663
Contributor III

We are facing 2 issues in our IMX6solo customised board.

  • Failure to resume from a Deep Sleep Mode
  • High Current in Deep Sleep Mode (~60mA)

After we checked the PMIC power rails with Reference design,

 we found VIN3 in our design used 3.3V as input which was generated SW2 of the PMIC. We are taking the VDDHIGH_IN O/P power from VGEN6. So this may cause the issue?

VIN3 also need to be power SYS_4V2 ??? as like all Switching regulator input?

Please find the snap shot of PMIC circuitry design of our project.

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

3,144 Views
ramesh6663
Contributor III

Hi Igor,

   Thanks for your help.

Regards,

Rameshkumar

0 Kudos
Reply

3,144 Views
igorpadykov
NXP Employee
NXP Employee

Hi ramesh

please check sect.2.7 Measuring points on the Freescale SABRE SD platform

AN4715 i.MX 6Solo Power Consumption Measurement

https://www.nxp.com/docs/en/application-note/AN4715.pdf 

for correct measurements, to check if ~60mA is for all board.

> we found VIN3 in our design used 3.3V as input which was generated SW2 of the PMIC.

>We are taking the VDDHIGH_IN O/P power from VGEN6. So this may cause the issue?

I do not think so

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply