IMX6SX Sabre Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6SX Sabre Board

3,492件の閲覧回数
raghavendraks
Contributor II

Hi,

Can anyone share the startup files for IMX6SX (Cortex-A9 & Cortex A9) board.

Regards,

Raghavendra

ラベル(2)
2 返答(返信)

3,190件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you need to test Uart under any OS? if you use linux, you can refer to the enclosed file, focus on the Chapter 45
Universal Asynchronous Receiver/Transmitter (UART) Driver

3,190件の閲覧回数
raghavendraks
Contributor II

Hi Joan Xie

Thanks for your reply.

Yes i want to test UART in windows with DS-5 development studio IDE.  Referring to the imx6q manual (CHAPTER: 64) " IMX6 Dual_6Quad Applications Processor Reference Manual - IMX6DQRM" which is attached here. 

I need to know what are the mandatory header files need to add and UART initialization code with respect to the imx6q sabrelite board. I have gone through my steps in the code development, now am able to build the code also in ARM DS-5 IDE but not getting transmission output in the terminal window , If you have sample UART code  for imx6q board please update to me because it may help me lot. Also I have attached my code here.

Best Regards,

Raghavendra 

0 件の賞賛
返信