IMX6SOLO interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SOLO interrupt

1,433 Views
lihao1993
Contributor I

I want to know which pins of IMX6SOLO can be used as an interrupt pin, and which tube feet can wake up IMX6SOLO from low-power mode

Labels (1)
1 Reply

1,359 Views
art
NXP Employee
NXP Employee

All of the i.MX6Solo pins that have the GPIO function multiplexed can be configured to operate as the GPIO interrupt source, and any of these interrupts can wake the processor up from low-power mode.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------