IMX6Q mipi LCD ghost image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q mipi LCD ghost image

3,314 Views
ivychend
Contributor I

      1、Basic information

cpu:IMX6Q  android:4.4.2   kernel:linux3.0.5     mipi interface ips LCD

2、problem description

After machine start, when I stay at an UI for more than three minutes. There will be an obvious ghost image(ghost shadow, in chinese:残影).Like stay at setting for 3 minutes

4F0B476D2624B34442B1707D7A735FB9.jpg

Then we can see the setting ghost image at the screen

B6548D9B2F32E055D640778C7414437D.jpg

How to solve this probem? Thanks

Labels (4)
0 Kudos
Reply
3 Replies

3,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

this could be related to this specific lcd usage (for example some

power up sequence is needed), so one can try to get support from

lcd vendor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,124 Views
ivychend
Contributor I

Hi igor

I have checked power up sequence and data written to LCD IC for many times. The IC vendor of LCD used the same data to write to screen and it worked fine. Difference is IC vendor use other platform. Furthermore, the LCD works fine in MTK platform. So, there may be some problems in imx6q DSI source code

0 Kudos
Reply

3,123 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

one can try to check lcd timings and adjust them in driver described

in Chapter 6 MIPI DSI Driver attached Linux Manual.

~igor

0 Kudos
Reply