IMX6Q and Nand flash interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q and Nand flash interface

1,553件の閲覧回数
jk1z
Contributor I

Hi,

I have a question regarding a NAND flash device with spare area greater than 512bytes.

I have noted the IMX6 reference manual, it says that the spare area per page is 512 bytes.

So IMX6Q does not support NAND with spare area greater than 512 bytes? Kindly confirm.

regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,396件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jk

yes manual is correct: max spare area per page is 512 bytes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------