IMX6Q SPI Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q SPI Speed

5,053 Views
brli
Contributor III

Hi,

Could you suggest how to improve SPI speed?

We are connecting LCD(320x240) device to IMX6Q SPI interface, but its data transfer speed is slow. detail as attached

Free for 9.5 us per 8 bytes during transferring 320*240*2 bytes data size.

Free for 245 ns per 8 bits during transferring 320*240*2 bytes data size.

How can i reduce these free time?

 

Thanks!

Br Li 

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

4,750 Views
igorpadykov
NXP Employee
NXP Employee

Hi br

max. ecspi frequency can be found in sect.4.12.2.1 ECSPI Master Mode Timing

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

So in software one can try to set its clock to max. available values and use

bursts configured by BURST_LENGTH field ECSPIx_CONREG register.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,652 Views
angelo_d
Senior Contributor I

Note that there are different speed limit if you only write on TX fifo or only read from RX,
at least so it seems (IMX6DQIEC.pdf 4.12.2.1)

RX  max speed seems 25Mhz for fast pad group, 18Mhz for slow group.

While for TX seems possible to reach 66Mhz.

Is this assumption correct ?

 

 

 

0 Kudos
Reply

4,750 Views
brli
Contributor III

Hi Igorpadykov,

Where can i set the BURST_LENGTH in Linux source code?

Thanks!

Br Li

0 Kudos
Reply

4,750 Views
igorpadykov
NXP Employee
NXP Employee

one can look at ecspi driver

spi-imx.c\spi\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor

0 Kudos
Reply

4,750 Views
brli
Contributor III

Hi Igorpadykov,

Modify the burst length can reduce the the 245ns free time per 8 bits,but my LCD device protocol specified is 8 bits transfer. otherwise it works abnormal.

Can we possible to reduce the 9.5 us free time per 8 bytes, or increase the 8 bytes to 16/24/32 bytes?

Thanks!

Br Li

0 Kudos
Reply