IMX6Q Android8.0 Ethernet Static IP Not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q Android8.0 Ethernet Static IP Not work

10,973 次查看
leavs
Contributor IV

Hi,

I have one imx6q device which run Android 8.0 system, I need to set Static IP, so I use com.fsl.ethernet to do that,

I can set the right IP, but I can't communication to other. I use follow command to test:

My Static IP:

```

IP: 192.168.6.99

Netmask: 255.255.255.0

DNS: 192.168.6.1

Gateway: 192.168.6.1

```

Error:

```

ping 192.168.6.1

Network is unreachable

ping www.google.com

Network is unkonw

```

I can get the prop is right:

```

sabresd_6dq:/ # getprop | grep dns
getprop | grep dns
[init.svc.mdnsd]: [running]
[net.dns1]: [192.168.6.1]
[net.eth0.dns1]: [192.168.6.1]
[net.eth0.dns2]: [0.0.0.0]
[ro.boottime.mdnsd]: [11647904667]

```

when I set the ethernet to dhcp, It work well.

can anyone know this problem?

标签 (1)
11 回复数

9,117 次查看
kwun9106
Contributor I

Someone solved this problem

Add some code in " /frameworks/opt/net/ethernet/java/com/android/server/ethernet/EthernetNetworkFactory.java "

https://www.jpand.me/2019/05/24/android-o-static-ip-trouble-shooting/ 

0 项奖励
回复

9,117 次查看
carloorsi
Contributor II

Hi,

I have the same issue!

I'm spending a lot of time without success.

Uff...

0 项奖励
回复

9,117 次查看
fensy
Contributor II

I tried to use network adb.

> ip route add default via 192.168.0.1

> setprop net.eth0.dns1 168.126.63.1
> setprop net.eth0.dns2 8.8.8.8

I could communicate with my pc, but I still could not access the internet.

0 项奖励
回复

9,117 次查看
carloorsi
Contributor II

I tried to evaluate differences between DHCP settings and STATIC.

I investigated with iproute2 tool.

Only difference is with ip rule show:

the first one is with STATIC, the second one with DHCP...

pastedImage_2.png

In STATIC are not present the rules to support eth0.

I believe this is the issue but I don't know how to solve.

I tried to add manually without success with:

ip rule add oif eth0 uidrange 0-0 lookup eth0

unfortunately last eth0 is a non valid argument...

Not only, I don't find the file

/etc/iproute2/rt_tables 

where official documentation suggest to see the valid argument for lookup (table).

 

0 项奖励
回复

9,117 次查看
carloorsi
Contributor II

Finally I solved!

You can set your favorite STATIC address and after to adjust configuration manually with ADB in root mode:

ip route add default via 192.168.1.1 dev eth0 table legacy_network

ndc resolver setnetdns eth0 . 8.8.8.8 8.8.4.4

Now the board can browse around Internet...

Modification is not permanent!!!

Next step will be to understand how to fix the bug in com.fsl.ethernet

Carlo

9,117 次查看
fensy
Contributor II

great!

I have used .sh in init.rc in the kitkat version.

ex)

init.rc

+service mysh /system/bin/sh /system/bin/network_init_eth0.sh
+   class late_start
+   oneshot

network_init_eth0.sh

+ifconfig eth0 192.6.94.200 netmask 255.255.255.0 up

+ip route add default gw 192.168.1.1 dev eth0

+ip route add default via 192.168.1.1 dev eth0 table legacy_network

+ndc resolver setnetdns eth0 . 8.8.8.8 8.8.4.4

+setprop net.eth0.dns1 168.126.63.1
+setprop net.eth0.dns2 8.8.8.8

In Android M version, need to add SELINUX policy.

0 项奖励
回复

9,117 次查看
fensy
Contributor II

Hi, 

I haven't found a solution yet, but i found the difference between DHCP and STATIC.

 

DHCP

#ip rule

0: from all lookup local
10000: from all fwmark 0xc0000/0xd0000 lookup legacy_system
13000: from all fwmark 0x10063/0x1ffff lookup local_network
15000: from all fwmark 0x0/0x10000 lookup legacy_system
16000: from all fwmark 0x0/0x10000 lookup legacy_network
17000: from all fwmark 0x0/0x10000 lookup local_network
23000: from all fwmark 0x0/0xffff uidrange 0-0 lookup main
32000: from all unreachable

13000: from all fwmark 0x10065/0x1ffff lookup eth0
19000: from all fwmark 0x65/0x1ffff lookup eth0
22000: from all fwmark 0x0/0xffff lookup eth0
14000: from all oif eth0 lookup eth0
10500: from all oif eth0 uidrange 0-0 lookup eth0

Static IP

0: from all lookup local
10000: from all fwmark 0xc0000/0xd0000 lookup legacy_system
13000: from all fwmark 0x10063/0x1ffff lookup local_network
15000: from all fwmark 0x0/0x10000 lookup legacy_system
16000: from all fwmark 0x0/0x10000 lookup legacy_network
17000: from all fwmark 0x0/0x10000 lookup local_network
23000: from all fwmark 0x0/0xffff uidrange 0-0 lookup main
32000: from all unreachable

If I know the difference, I think I can find a way.

0 项奖励
回复

9,117 次查看
diegoadrian
NXP Employee
NXP Employee

Hello

I apologize for the delay.

Have you tried to set up the static ip as the below video?

How to Set Static IP Address on Android 4 (Ice-Cream) - YouTube 

Hope it can help you.

Best Regards,

Diego.

0 项奖励
回复

9,117 次查看
leavs
Contributor IV

Hi Diego,

If there is one patch to fix this issue?

0 项奖励
回复

9,117 次查看
leavs
Contributor IV

Hi,

Thanks for your reply.

I tested the static IP config of WIFI, It can work well.

But I need the ethernet to set static IP feature, I use the ethernet.apk from fsl, It can set static ip, but I can't comunication with ethernet.

The ethernet.apk run ok in android 6.0 from nxp.

Is there some bugs for ethernet.apk in Android8.0 ?

0 项奖励
回复

9,117 次查看
leavs
Contributor IV

are there anyone know this problem?

0 项奖励
回复