IMX6DQ Android 9 high CPU usage when watching youtube

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DQ Android 9 high CPU usage when watching youtube

3,248 Views
TCLin
Contributor II

Hi,

I got high CPU usage when watching youtube.

CPU always stays above 80% and even exceeds 100%

TCLin_0-1608020887901.png

 

 

0 Kudos
Reply
4 Replies

3,201 Views
TCLin
Contributor II

Did anyone meet the same problem?

0 Kudos
Reply

3,244 Views
igorpadykov
NXP Employee
NXP Employee

Hi TCLin

 

one can try to test browser hardware acceleration using sect.5.6.5 Chromium Browser 

i.MX Yocto Project User’s Guide​

 

Best regards
igor

0 Kudos
Reply

3,219 Views
TCLin
Contributor II

 

I got the same problem in different web view app (Chrome,Firefox,Edge) 

Does anyone have the same experience?

How do I resolve this problem?

Thank you for your help

0 Kudos
Reply

3,239 Views
TCLin
Contributor II

I can't use the User's Guide you provide because I am using android 9

0 Kudos
Reply