IMX6DP and isl79987 video: image scrolling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6DP and isl79987 video: image scrolling

381件の閲覧回数
vaudoitlaurent
Contributor IV

Hi all,

we are using on a custom board an imx6dp with isl79987 chip.

We are based on yocto warrior fsl release (kernel 4.19, yocto warrior).

 

i have applied the patch found here (https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX6DQ-ISL79985-79987-MIPI-CSI2-CVBS-cam...) , to allow display 4 camera.

It works well and i'm able to launch  mxc_v4l2_tvin (up to 4 times to display 4 camera channel).

Anyway, sometimes after a while, one channel video scroll until it get resynchonized.

When it happens, i have the message

IPU WARNING IPU_INT_STAT_5=0x00000001

I've check that the isl has no error (by checking status register for each channel).

Would you have an idea of what i could check to find the problem?

 

Thanks in advance

Best regards

Laurent

 

 

 

0 件の賞賛
返信
1 返信

359件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @vaudoitlaurent,

I hope you are doing well.

One possible reason for this issue could be the video data frame buffer.

Could you please confirm if the data is being transferred to the same frame buffer? If yes, the frame buffer must be over-flowed.

 

Thank you.
Best Regards,
Dhruvit.

0 件の賞賛
返信