IMX6DL android5.0 HDMI has no sound!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL android5.0 HDMI has no sound!!!

975 Views
尚飞汤
Contributor IV

First our HDMI has no sound,when i check the cmdline dev=hdmi,1280*1080M@60 not the same like the device tree,the device tree is 1920*1080M@60,

I change the cmd line to 1920*1080M@60, the HDMI sound is ok.

can anyone tell me why????????how could the HDMI resolution affect the audio????

Tags (2)
0 Kudos
Reply
3 Replies

842 Views
igorpadykov
NXP Employee
NXP Employee

Hi

right, audio can be affected as it is sent with

hdmi signal. Correct hdmi clock should be selected for

using audio, please check sect.33.4.3 Supported Video Mode

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

842 Views
尚飞汤
Contributor IV

Dear Igorpadykov:

I understand the question,the 1280*800 mode is not in the mode list been supported.

and the HDMI resolution should the same as the device set.

however , on android 4.2 we use the resolution ,the audio is okay.

0 Kudos
Reply

842 Views
尚飞汤
Contributor IV

Dear Igorpadykov:

do you mean the 1280*800M@60 is not in the supported mode list?

However i don't understand should't the hdmi mode be setted by the edid massage?

by the way,the cmdline used on the android 4.2 version is ok,but android 5.0 has the device tree is bad.

i just can't understand why?

0 Kudos
Reply