IMX6 uboot fuse command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 uboot fuse command

2,682 Views
liuhao1
Contributor II

I want write some value to fuse

In uboot I try "fuse prog 3 0 xxxx"

And then I use "fuse read 3 0", out put 0

It seem the command did not take effect

Before I need to use "fuse prog 3 0" , Any pre-operation such as the need to do other bits to be rewritten?

0 Kudos
Reply
1 Reply

2,308 Views
igorpadykov
NXP Employee
NXP Employee

Hi 浩 刘

fuses may be locked, please check Table Lock Fuses in Chapter
Fusemap Reference Manual processor which are you using.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------