IMX6 solo bluetooth uart abnormal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 solo bluetooth uart abnormal

1,649件の閲覧回数
garyyin
Contributor III

i.mx 6 solo, linux 3.10.45

When the following message appears, the sound of the bluetooth phone becomes abnormal.

fsl-ssi-dai 202c000.ssi: slot number should be >= 2 in I2S or NET
imx-uart 21f4000.serial: Rx FIFO overrun
fsl-ssi-dai 202c000.ssi: slot number should be >= 2 in I2S or NET

imx-uart 21f4000.serial: Rx FIFO overrun

... ...

ラベル(4)
タグ(4)
0 件の賞賛
返信
1 返信

1,462件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gary

linux 3.10.45 is not supported by nxp, please try latest nxp bsps from:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信