IMX6 series Wifi selection.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 series Wifi selection.

4,771件の閲覧回数
du_minglei
Contributor I

Which WiFi modules does the imx6 series support? Can you list some? Must be debugged on the IMX6 platform.i.MX Processors‌

ラベル(3)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

4,274件の閲覧回数
romitchatterjee
Contributor V

Hello Kevin,

I hope you found what you were looking for at https://wireless.murata.com/products/rf-modules-1/wi-fi-bluetooth-for-nxp-i-mx.html? Do you have any specific application in mind?

Thanks.

0 件の賞賛
返信

4,269件の閲覧回数
du_minglei
Contributor I

Thank you very much!

Kind regards

Kevin

Kevin

+86 15856950049

[email protected]

Geniatech Anhui LLC

Room 906,Building F5,Innovation Industrial Park,NO.2800 InnovationRoad,High Tech Zone,Hefei,Anhui,China

www.geniatech.com

0 件の賞賛
返信

4,269件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can see that the default WIFI support is Broadcom BCM4339 in hardware. In our linux and android released BSP documents you can see. Also you can look at i.mx wifi modules description on

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Hope this can do help for you
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信