IMX6 security reference manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 security reference manual

3,636件の閲覧回数
jacques
Contributor I

Hello,

I have the imx6 security reference manual, but it only covers the chips Dual, Qual, Solo and DualLite.

Where can I get information about the security features of other chips in the imx6 family?

According to this:

http://cache.freescale.com/files/32bit/doc/brochure/FLYRIMXPRDCMPR.pdf

for instance the imx6 UltraLite has some different security functionalities.

Thank you,

Jacques

0 件の賞賛
返信
1 返信

1,951件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jacques

these documents can be obtained from local FAE,

note one needs to have NDA

1.jpg

i.MX 6UltraLite Applications Processor|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信