IMX6 hardware codec support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 hardware codec support

2,516 次查看
lyfsci
Contributor III

Hi Experts,

What are all the hardware based video/audio codecs which was supported in the IMX6 platforms ?

Regards,

Lyf

标签 (1)
0 项奖励
回复
1 回复

2,087 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lyf

codec specs are provided in Release Notes included in Linux Doc package,

for example in attached L3.14.52 document sect.6.5 Multimedia feature matrix,

which can be obtained from

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复