IMX6 hardware codec support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 hardware codec support

2,513 Views
lyfsci
Contributor III

Hi Experts,

What are all the hardware based video/audio codecs which was supported in the IMX6 platforms ?

Regards,

Lyf

Labels (1)
0 Kudos
Reply
1 Reply

2,084 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

codec specs are provided in Release Notes included in Linux Doc package,

for example in attached L3.14.52 document sect.6.5 Multimedia feature matrix,

which can be obtained from

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply