IMX6 frame number limitations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 frame number limitations

1,340件の閲覧回数
ashokp
Contributor I

Hi All,

Is there any frame limitations in iMX6. When analysing the code i saw the frame number is hardcoded to 10 in the below file

drivers/media/platform/mxc/capture/mxc_v4l2_capture.h

#define FRAME_NUM 10

Please let me know wheather iMX6 can handle more than 10 frames

Thanks,

P.Ashok

ラベル(7)
0 件の賞賛
返信
1 返信

1,271件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ashok

yes more than 10 frames can be used, as this is temporary

buffer for processing incoming data.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信