IMX6 bayer to RGB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 bayer to RGB

1,808 次查看
prasadadireddy
Contributor I

Hi,

We are using Aptina  sensor (mt9p031) and interfaced with csi parallel bus. My sensor output gives bayer RGB (GRGB format) height & width = 2580X1944. I am able to display monochrome image with 15 fps.

Using opencv I am able to convert bayer to RGB, but it's not meeting our requirement (i.e., FPS is too low). I know IMX6 doesn't have ISP, so I planned to implement  demosaicing algoritim at driver level.

Please suggest is it possible to implement at driver level, if yes please share the required modifications..

0 项奖励
回复
1 回复

1,668 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi prasad,

.MX6 IPU don't make Bayer conversion. You will need to use some graphics library/API like gstreamer, ffmpeg and others to make this conversion using the CPU. IPU (IC, DP, DC and etc) doesn't recognize bayer as a valid image format. It can receive bayer format from CSI port as generic data.

I have this capture driver (using the IPU) and used the following code to map the DMA memory (from IPU) to user space: Normally because of DMA memory is mapped uncached, but due to size and usage, it's no problem to map it cached.

 

/* function to map DMA memory to user space */

static int capture_mmap(struct file *file, struct vm_area_struct *vm)

{

   struct capture_device *dev = file->private_data;

   size_t rsize = vm->vm_end - vm->vm_start;

   int map;

   int idx;

 

   if ((vm->vm_pgoff * PAGE_SIZE) != (unsigned long)dev->dma)

      return -ENOMEM;           /* wrong base address */

    if (down_interruptible(&dev->busy_lock))

      return -EINTR;

 

   vm->vm_page_prot = phys_mem_access_prot(file, vm->vm_pgoff, rsize, vm->vm_page_prot);

   /* map DMA memory to user process (allow cacheable, since data much larger than cache) */

   if (remap_pfn_range(vm, vm->vm_start, vm->vm_pgoff, rsize, vm->vm_page_prot))

      map = EAGAIN;

   else

      map = 0;

   up(&dev->busy_lock);

   return map;

}

 

If you use some driver from NXP, you may have to change the driver.

 

Regards

0 项奖励
回复