IMX6 UL PIN MULTIPLEXING

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 UL PIN MULTIPLEXING

1,951 次查看
Hamza_Hassan
Contributor I

Hi

I am using IMX6.UL processor pin . I am using RS232 transmitter using serial port. Can i use the same pin as GPIO for transmitting IR signal.

Is there any support in IMX6?

Please guide me on this.

 

Thanks

0 项奖励
回复
3 回复数

1,932 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Hamza_Hassan,

Hope you are doing well.

One can check the Available mux options of the pin which is configured as a RS232 Transmitter in RM. If the possible pad is GPIO*, then you can configure the same pin as a GPIO for transmitting IR signal.
Please note that once you configure this pin as a GPIO, After that you will not be able to use the same pin as Rs232 Transmitter.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复

1,905 次查看
Hamza_Hassan
Contributor I

Hi @riteshmpatel ,

Hope you are doing well.

Can I configure the pin at runtime?

Or should I need to reboot every time for new configuration?

Thanks

Hamza Hassan

0 项奖励
回复

1,896 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Hamza_Hassan,

Unforutnately, doing runtime configurations is not possible.

The configurations must be done in dts.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复