IMX6 UL ADC in devicetree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 UL ADC in devicetree

7,007 Views
podarce
Contributor I

I would like to use the ADC1 with in1, in2 and in4 channels.

On the DeviceTree source (.dts) I wrote:

&adc1 {
    vref-supply = <&touch_3v3_regulator>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_adc1>;
    clocks = <&clks IMX6UL_CLK_PWM8>,
        <&clks IMX6UL_CLK_PWM8>;
    num-channels = <3>;
    status = "okay";
};

  pinctrl_adc1: adc1grp {
            fsl,pins = <
                MX6UL_PAD_GPIO1_IO01__GPIO1_IO01    0x000b0  /* ADC1_IN1  */
                MX6UL_PAD_GPIO1_IO02__GPIO1_IO02    0x000b0  /* ADC1_IN2  */
                MX6UL_PAD_GPIO1_IO04__GPIO1_IO04    0x000b0  /* ADC1_IN4  */
            >;
        };

while in the included imx6ul.dtsi (not edited) I have:

adc1: adc@02198000 {
                compatible = "fsl,imx6ul-adc", "fsl,vf610-adc";
                reg = <0x02198000 0x4000>;
                interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
                clocks = <&clks IMX6UL_CLK_ADC1>;
                num-channels = <2>;
                clock-names = "adc";
                status = "disabled";
                        };

When I take a look to the sysfs of my linux distro, I can only see 2 adc channels (in_voltage0_raw and in_voltage1_raw) and if I try to read their values i get the "Connection Timed Out" error.

How could I fix it ?

Regards.

UPDATE: Setting num-channels = <3> in the imx6ul.dtsi file allows to see 3 in_voltageX_raw items in my sysfs.

I supposed the dts file overlayered the included file, so I can't figure it out.

The problem of Connection Timed Our persists.

Labels (3)
0 Kudos
Reply
2 Replies

4,730 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniele

seems record num-channels  should not be duplicated in dts and dtsi, as example one can look at :

 imx6ull-14x14-ddr3-arm2-adc.dts
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6ull-14x14-ddr3-ar...
&adc1 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_adc1>;
    vref-supply = <&reg_vref_3v3>;
    status = "okay";
};
imx6ull.dtsi
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6ull.dtsi?h=imx_4....
            adc1: adc@02198000 {
                compatible = "fsl,imx6ul-adc", "fsl,vf610-adc";
                reg = <0x02198000 0x4000>;
                interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
                clocks = <&clks IMX6UL_CLK_ADC1>;
                num-channels = <2>;
                clock-names = "adc";
                status = "disabled";
                        };

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,730 Views
jeremy_cole
Contributor I

Hi, I am having a similar problem, on an IMX6ULL EVK board. I am using GPIO pins 0 - 3 for digital I/O, and I want to use GPIO1_IO04 as an analog input (ADC1_IN4). I added this to my board DTS file:

&adc1 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_adc1>;
    num-channels = <5>;
    status = "ok";
};

And:

        pinctrl_adc1: adc1grp {
            fsl,pins = <
                MX6UL_PAD_GPIO1_IO04__GPIO1_IO04    0x00080  /* ADC1_IN4  */
            >;
        };

This works and I see 5 input channels under "/sys/bus/iio/devices/iio\:device0/", in_voltage0_raw to in_voltage4_raw.

By setting analog voltages on various pins and reading the values, I have confirmed that at least GPIO_1 and GPIO_4 are working as analog channels (other pins are used for other things so just read high or low).

However, this seems incorrect if I ONLY want one analog input channel. What should I use in the DTS file if I want only one ADC input channel in iio:device0, connected to the ADC1_IN4 pin?

Nb: If I remove "num-channels = <5>" from my DTS, I get the (default) 2 channels and they are connected to GPIO pins 0 and 1.

0 Kudos
Reply