IMX6 Sabre board - USB Host Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Sabre board - USB Host Mode

1,707 Views
jhtate1
Contributor I

Hello support,

We need 2 USB ports, one is for android debugging and one is for mouse or touch controller connected.  

How can we install the USB host device on top of IMX6 Sabre board.

Also we need to know how to change the linux kernel to enable imx6’s usb host.

Thank you

0 Kudos
Reply
1 Reply

1,424 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to Linux documentation about USB :

Chapter 10 of “i.MX_BSP_Porting_Guide.pdf” ;

Chapter 39 (CHIPIDEA USB Driver) of “i.MX_Linux_Reference_Manual.pdf”.

 

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply