IMX6 Quad : VPU Capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Quad : VPU Capability

2,054件の閲覧回数
anjojohn
Contributor IV
Hi all 
We need  clarification for IMX6 Quad capability for H264 encoding/decoding. Our requirement is to encode and decode 1080p30 video at the same time (2 way video call). Is IMX6 Quad enough for this ? Currently we are using IMX6 Dualite which can only encode or decode 1080p30(not at same time).
0 件の賞賛
返信
3 返答(返信)

1,760件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  That is extreme load - two (encode + decode) streams of 1080p@30

for i.MX6 VPU -  not supported. 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

0 件の賞賛
返信

1,760件の閲覧回数
anjojohn
Contributor IV

Hi Yuri,

Thank you for the quick response. If we could reduce the use-case  to 1080p30 encoding and 720p decoding at the same time, can this be possible . Also forgot to mention we have Full HD display in Dual LVDS and one down-scaling of 1080p30 stream to VGA.

0 件の賞賛
返信

1,760件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

use-case  to 1080p30 encoding and 720p decoding at the same time is possible.

Regards,

Yuri.

0 件の賞賛
返信