IMX6 PCIE Statistics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 PCIE Statistics

1,574 Views
ieio
Contributor IV

Hi all,

I am working to pcie with imx6 in Linux.

I noticed that IBM s390 has a nice feature that you can enable to show pcie statistics: https://www.ibm.com/support/knowledgecenter/en/linuxonibm/com.ibm.linux.z.lgdd/lgdd_t_pcie_work_stat..., I was wondering if can be done the same for imx6.

I gave a look to PCI RC registers but I didn't find anything useful.

Is there a way to get these statistics or at least the AER ones?

Thanks in advance.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,503 Views
igorpadykov
NXP Employee
NXP Employee

Hi ieio

I am afraid such tool is not available for i.mx6 pcie, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply