IMX6: Not using HDMI and PCIe; Do I still have power them?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6: Not using HDMI and PCIe; Do I still have power them?

642件の閲覧回数
michaelbazarov
Contributor II

Reference manual talks about power collapsing for the HDMI PHY: short all data and clocks to GND. Says there is no constraint on power supply sequence when not using HDMI which seems to imply we don't have to connect VDD HIGH CAP and VDD SOC CAP and associated decoupling to the HDMI VP and VPH rails. Can someone confirm that?

Unable to find anything about how to power the PCIe bus if we don't intend to use it.

0 件の賞賛
返信
1 返信

507件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi michael

please look at sect.2.8 Unused analog interfaces IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信