IMX6: Not using HDMI and PCIe; Do I still have power them?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6: Not using HDMI and PCIe; Do I still have power them?

496 次查看
michaelbazarov
Contributor II

Reference manual talks about power collapsing for the HDMI PHY: short all data and clocks to GND. Says there is no constraint on power supply sequence when not using HDMI which seems to imply we don't have to connect VDD HIGH CAP and VDD SOC CAP and associated decoupling to the HDMI VP and VPH rails. Can someone confirm that?

Unable to find anything about how to power the PCIe bus if we don't intend to use it.

0 项奖励
1 回复

361 次查看
igorpadykov
NXP Employee
NXP Employee

Hi michael

please look at sect.2.8 Unused analog interfaces IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励