IMX6 FT2232H OpenOCD config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 FT2232H OpenOCD config

2,967 Views
Alex_Smart
Contributor II

I have a IMX6 quad Sabreboard and trying to connect to this piece of equipment with OpenOCD via FT2232H based debugger. However, no luck so far.

Here is OpenOCD output:

 

openocd -f interface/ftdi/ft2232h.cfg -f board/fsl_imx6q_sabresd.cfg
Open On-Chip Debugger 0.12.0 (2024-09-16) [https://github.com/sysprogs/openocd]
Licensed under GNU GPL v2
libusb1 d52e355daa09f17ce64819122cb067b8a2ee0d4b
For bug reports, read
        http://openocd.org/doc/doxygen/bugs.html
DEPRECATED! use 'adapter driver' not 'interface'
DEPRECATED! use 'ftdi vid_pid' not 'ftdi_vid_pid'
DEPRECATED! use 'ftdi channel' not 'ftdi_channel'
DEPRECATED! use 'ftdi layout_init' not 'ftdi_layout_init'
DEPRECATED! use 'adapter speed' not 'adapter_khz'
adapter speed: 200 kHz
Warn : Transport "jtag" was already selected
Warn : imx6q.sdma: nonstandard IR value
../OpenOCD-20240916-0.12.0/bin/../share/openocd/scripts/board/fsl_imx6q_sabresd.cfg:145: Error: invalid command name "imx6q.cpu.0.0"
in procedure 'script'
at file "embedded:startup.tcl", line 28
at file "../OpenOCD-20240916-0.12.0/bin/../share/openocd/scripts/board/fsl_imx6q_sabresd.cfg", line 145

I read this topic, and this is basically what I need https://community.nxp.com/t5/i-MX-Processors/How-to-burn-U-boot-using-JTAG-for-IMX6Q/m-p/985128

but that solution didnt wotk either.

Is there some other cfg files or something?

Labels (1)
0 Kudos
Reply
2 Replies

2,939 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,919 Views
Alex_Smart
Contributor II

Thanks. It did help and I found a Jlink. Now there is a different issue: JTAG-DP STICKY ERROR

Open On-Chip Debugger 0.12.0 (2024-09-16) [https://github.com/sysprogs/openocd]
Licensed under GNU GPL v2
libusb1 d52e355daa09f17ce64819122cb067b8a2ee0d4b
For bug reports, read
        http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
Warn : imx6.sdma: nonstandard IR value
Info : Hardware thread awareness created
Info : Hardware thread awareness created
Info : Hardware thread awareness created
Info : Hardware thread awareness created
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : J-Link ARM V8 compiled Jun 19 2012 11:29:30
Info : Hardware version: 8.00
Info : VTarget = 3.306 V
Info : clock speed 1000 kHz
Info : JTAG tap: imx6.cpu tap/device found: 0x4ba00477 (mfg: 0x23b (ARM Ltd), part: 0xba00, ver: 0x4)
Info : TAP imx6.sdma does not have valid IDCODE (idcode=0x4323803a)
Info : JTAG tap: imx6.sjc tap/device found: 0x2191c01d (mfg: 0x00e (Freescale (Motorola)), part: 0x191c, ver: 0x2)
Error: JTAG-DP STICKY ERROR
Error: [imx6.cpu.0] Examination failed
Warn : target imx6.cpu.0 examination failed
Error: JTAG-DP STICKY ERROR
Error: [imx6.cpu.1] Examination failed
Warn : target imx6.cpu.1 examination failed
Error: JTAG-DP STICKY ERROR
Error: [imx6.cpu.2] Examination failed
Warn : target imx6.cpu.2 examination failed
Error: JTAG-DP STICKY ERROR
Error: [imx6.cpu.3] Examination failed
Warn : target imx6.cpu.3 examination failed
Info : [imx6.cpu.0] starting gdb server on 3333
Info : Listening on port 3333 for gdb connections

 What is that?

0 Kudos
Reply