What are the requirements on the OOB area when writing the FCB block? Can I write whatever I want in the OOB area associated with the FCB block or does it have to be empty?
I understand, but it would be really nice to know if I am allowed to put other information in the OOB area of the FCB block? Also do I really have to write the FCB block with raw write? Or can I write it with standard ECC?
Hello,
i.MX6 specifics are shown in section 8.5.2.5 (Bad Block Handling in the ROM)
of i.MX6 D/Q RM.
Regards,
Yuri.
Hello,
It is highly recommended to use the kobs-ng utility for writing NAND FCB.
Please refer to MFG tool "NAND Flash" configuration in ucl2.xml
Kong-ng is part of NXP Linux BSP.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!