IMX6 Dual Processor ISSUE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Dual Processor ISSUE

2,106 Views
ronakkotak
Contributor I

I am using IMX6 Dual processor in my current project.

My PCB Size is 1mm thick,When i power up the system processor heats too much within 5-10 minutes.

Is this normal issue or something to worry about.Please guide me.

Labels (1)
0 Kudos
Reply
3 Replies

1,960 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ronak

booting up to Uboot without enabled caches, processor is not hot.

However when you enabled caches and boot Linux it may be hot.

If playing video or using graphics engine (GPU) it may be more hot.

You can look below for background:

AN4509 i.MX 6Dual/6Quad Power Consumption Measurement

AN4579 i.MX 6 Series Thermal Management Guidelines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,960 Views
ronakkotak
Contributor I

I am using the same series processor in my previous design.

The difference between previous and present design is just PCB thickness rest all is same.

In my previous design it was not heating too much as of now.

0 Kudos
Reply

1,959 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ronak

you can measure current in both cases and compare.

Best regards

igor

0 Kudos
Reply