[IMX6] Change Audio card on Android 7 using Sabresd Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[IMX6] Change Audio card on Android 7 using Sabresd Board

3,471 次查看
mayqueen
Contributor IV

Hello All:

As title, I boot success on Android 7 using HDMI mode, but the default audio card is wm8962 audio codec, so it's so creepy when I control the HDMI monitor but the sound output is from wm8962 speaker.

Anybody know how to change the default audio card on Android, I think maybe modify tinyalsa source on HAL layer?

Thank you!

标签 (3)
4 回复数

2,709 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The following may help.

https://community.nxp.com/docs/DOC-93745 

Regards,

Yuri.

0 项奖励
回复

2,709 次查看
gary_bisson
Senior Contributor III

Hi,

You can look at the patch below which does just that:

tinyalsa: allow HDMI to be used as primary output/input device · boundarydevices/android_hardware_im... 

With that patch, if you set one property to 1 then the audio will go to HDMI:

$ setprop persist.audio.hdmi_out 1

Note that this property is persisten across reboot, you only need to set it once.

Regards,

Gary

2,709 次查看
mayqueen
Contributor IV

Awesome! thanks! BD is really a powerful contributor!

0 项奖励
回复

2,709 次查看
wangxizhi
Contributor I

HI  May Queen:

I have some questions about  IMX6 SABRE board,  I port android N 7.1.1  with  IMX6 SABRE board(cpu imx6qp), Both the development board and the code are provided by NXP , I think the development board should work properly . but my code have so many problems? I think it must be something wrong with my operation,I want to know if there were any problems when you debug the source code,Can you give me some reference about how to port android N 7.1.1  with  IMX6 SABRE board? I looked at the documentation for the android_N7.1.1_1.0.0_docs folder, but it still didn't work out,Thank you very much!

0 项奖励
回复