IMX6 Booting using SPI NAND FLASH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Booting using SPI NAND FLASH

2,641 Views
shammi112
Contributor I

Hello.

Can i boot imx6 using SPI based NAND FLASH M29F4G01ADAGDSF-IT ?

Regards,

SHAMMI

0 Kudos
Reply
3 Replies

2,293 Views
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

unfortunately boot from SPI based NAND is not supported by i.MX6DQ

according to boot options described in Chapter 8 System Boot i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,293 Views
shammi112
Contributor I

hi,

Thanks for reply. Can be boot using MT29F128G08AJAAAWP  GPMI NAND FLASH, having 8k page size ?

Regards,

SHAMMI

0 Kudos
Reply

2,293 Views
igorpadykov
NXP Employee
NXP Employee

yes, booting from parallel nands with 8k page size is supported.

~igor

0 Kudos
Reply