IMX53QSB boot from SATA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53QSB boot from SATA

Jump to solution
1,901 Views
mackwarren
Contributor I

I'm having trouble finding instruction how to create the yocto and uboot image for booting directly from sata. Has anyone accomplished this?

0 Kudos
Reply
1 Solution
1,761 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mac

first enable internal clock for SATA blowing fuse:

iim blow 4 3 4

1.jpg

then follow similar procedure for i.MX6

Re: SATA and u-boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,762 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mac

first enable internal clock for SATA blowing fuse:

iim blow 4 3 4

1.jpg

then follow similar procedure for i.MX6

Re: SATA and u-boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,761 Views
TomE
Specialist II

Hardware Reference Manual for i.MX53 Quick Start

5.4.2. Boot Mode Operations and Selections

Do you know that you have to install a DIP switch on the board, and remove and rearrange a whole bunch of resistors in order to select a SATA boot?

Tom

0 Kudos
Reply